Other Parts Discussed in Thread: MSP430F5324, MSP430F5310
Dear all,
When I use bit-fields in MSP430F5301-MSP430F5310, MSP4305501-MSP430F5510, the compiler will give error. The error is as following.
"Fatal Error[e72]: Segment DATA20_Z must be defined in a segment definition option (-Z, -b or -P) ".
My compiler is IAR for MSP430 V5.30. But to be stranged, when choose other MCUs ,for examples MSP430F5324 or MSP4305438, the will be no error.
The "Data model" is selected "Large".
Just like the the following test project, the compiler will give error
typedef struct {
MUINT16 i:1;
MUINT16 j:1;
MUINT16 k:1;
MUINT16 l:1;
MUINT16 m:1;
MUINT16 n:1;
MUINT16 iiii :10;
}tSchedule;
void main(void)
{
tSchedule tmp;
tmp.i =0;
}
Any comments will be appreciated