Other Parts Discussed in Thread: MSP430FR5739
Hi,
I am using MSP430FR5739 with example codes. i configure the uart 9600 baud rate, but when i want to see the transmitted data on putty.exe or CommOperator it shows the true data on 2400 baud rate. The code is given below. Please help
P2SEL1 |= BIT0 + BIT1;
P2SEL0 &= ~(BIT0 + BIT1);
UCA0CTL1 |= UCSWRST;
UCA0CTL1 = UCSSEL_1; // Set ACLK = 32768 as UCBRCLK
UCA0BR0 = 3; // 9600 baud
UCA0MCTLW |= 0x5300; // 32768/9600 - INT(32768/9600)=0.41
// UCBRSx value = 0x53 (See UG)
UCA0BR1 = 0;
UCA0CTL1 &= ~UCSWRST; // release from reset
UCA0IE |= UCRXIE; // enable RX interrupt