This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For some reason cannot stop DCO while using VLO
BCSCTL3 |= LFXT1S_2;
BCSCTL2 |= SELM_3 + DIVM_1;
__bis_SR_register(SCG1 + SCG0); - this command does not work.
MCLK is using VLO, Timer is clocked by VLO too - both statements are verified. Goal is to achieve tens of microamps current consumption, nothing else is connected.
Current is around 180uA no matter how timer is clocked via DCO - SMCLK or VLO - ACLK (verified by checking output frequencies in both cases).
There is no difference with or without __bis__SR_register(SCG0 + SCG1) command line.
My conclusion about DCO running in both case came from the same current consumption and no impact after SCG0/SCG1 setting.
Yes. That's what I wrote. As long as SMCLK still requires DCO, setting SCG0 has no effect and DCO remains active. You need to switch SMCLK to VLO too and then DCO can be deactivated by SCG0.
Setting both, SCG0 and SCG1 should switch SMCLK off and allow DCO to be shut down too. However, SMCLK cannot be disabled if anyone is still using it (SMCLK_request). Fig. 5-5 in the users guide shows that an SMCLK request (by any peripheral module) overrides the SCG0 and SCG1 bits.
Ok, I have tried the following:
BCSCTL3 |= LFXT1S_2; // ACLK=VLOCLK
BCSCTL2 |= SELM_3 + DIVM_1 + SELS + DIVS_3; // MCLK=VLOCLK/2, SMCLK=VLOCLK/8
__bis_SR_register(SCG1 + SCG0); // stop DCO
TACTL = TASSEL_1 + MC_1; // ACLK, UP mode
Still 180uA consumption.
That's strange.
Maybe DCO is off and the current is consumed by something else?
Unconnected (floating) input pins will draw lots of cross-currents if the input voltage is near the transition voltage. ULP advisor suggests putting all unused port pins to low output.
Also, even though ACLK is sourced by VLO, the XT1 circuit may still try to fire-up the XT1 crystal. YOu should also set the OSCOFF bit to really switch the oscillator off.
Still there, solid 180uA.
All P1 and P2 pins are connected: 3 P1 pins are configured as inputs and pulled up, the rest of are configured as outputs; P2 pins are configured as outputs. Touching any GPIOs does not change current, usually it will change if pin is floating.
P1DIR |= 0x7C;
P1REN |= 0x83;
P1IES |= 0x83;
P1IE |= 0x83;
P1SEL |= 0x04;
P2DIR |= 0xC0;
P2SEL &= ~(0xC0);
P2OUT = 0x00;
OSCOFF killed everything since it controls VLOCLK (5.2.2)
Ah, you're right, on 2x family, VLO is a direct replacement for LFXT1, as 2x family doesn't have REFO.Igor Radutnuy said:OSCOFF killed everything since it controls VLOCLK (5.2.2)
Not necessarily. The problem with floating pins is that if the input voltage is near the input gate level transition voltage, there will be significant cross-currents through the input gate transistors. These are independent of any leakage current in or out the pin. THis also happens if you oput out your ADC reference externally and then switch the reference off. The slowly lowering voltage on the external reference capacitors will eventually reach teh critical level and suddenly current consumption on the (sleeping) MSP begins to rise and hten falls again some time after..Igor Radutnuy said:Touching any GPIOs does not change current, usually it will change if pin is floating.
After weekend investigations I am now down to 100uA by reducing CPU clock (ACLK/8). Used blocks are: counting down CPU and timer A (also clocked by ACLK/8). Seems DCO is off because it consumes by itself around 200uA per specifications. Now I am wondering what is the lowest achievable current consumption for CPU clocked out by VLO? Same question for timer.
Regards.
??? CPU runs from MCLK and is independent of ACLK (even though both can be source by the same oscillator).Igor Radutnuy said:reducing CPU clock (ACLK/8)
Yes, MCLK = ACLK and then I have changed MCLK divider.
I build separate HW setup for current consumption investigation, only reset pin is connected to VDD and P1.1,2,7 connected to buttons.
It would be helpful to know bottom line of current consumption in VLO mode, I could not find any document about, also MSPs are advertised to have lowest power consumption.
Well, I more than once explained that low power consumption isn't a matter of 'I want it to be that low' but of 'I need this featuer and don't need that'.Igor Radutnuy said:I could not find any document about, also MSPs are advertised to have lowest power consumption.
However, it should be possible to reproduce the values in the datasheet by reconstructing the specific parameters with which these values have been originally measured.
What about pullups on the button pins? If present, then maximum curent on these three pions should be 150pA leakage.Igor Radutnuy said:only reset pin is connected to VDD and P1.1,2,7 connected to buttons.
Well MCLK and ACLK are parallel and independent. You cannot set MCLK to ACLK. But you can set both, MCLK and ACLK to the same oscillator, what probably is what you meant.Igor Radutnuy said:Yes, MCLK = ACLK and then I have changed MCLK divider.
However, the datasheet lists 65µA for CPU active mode with DCO on at 100kHz. (fACLK = 0Hz, fMCLK=fSMCLK=fDCO(0,0)=100kHz)
Well, teh dazasheet lists teh conditions for another state:
fMCLK=fSMCLK=fACLK=32768Hz/8 = 4kHz:
SELM_3, SELS, DIVM_3, DIVS_3, DIVA_3, SCG0=1, SCG0=0. CPU active. -> <7µA. Without crystal. VLO should be active. Power consumption might be a bit higher (since the oscillator will still try to fire up the crystal) but not too much (you may lower XT1 drive strength to minimum)
DCO mode is quite well characterized and reflected in datasheet, however VLO mode (featured as the lowest power consumption after crystal) is not. Power consumption must be clearly stated along with appropriate commands somewhere. I am RF guy and have moved in years around 30000 MSP430s, however never get attention from TI application support due to low volume I guess. All I need to know - are limits for VLO mode like 65uA @ 100kHz for DCO mode.
SELM_3, SELS, DIVM_3, DIVS_3, DIVA_3, SCG0=1, SCG0=0. CPU active. -> <7µA. Have tried this, still 100uA.
VLO ranges between 4 and 20kHz, and power consumption of VLO-driven CPU will change with it. So no specific value can be given. Originally VLO isn't meant to drive the CPU but to provide an emergency clock when the CPU is on sleep and nothing else is there to wake it.Igor Radutnuy said:VLO mode (featured as the lowest power consumption after crystal) is not.
The question remains: why isn't your current as low as it should. I don't know. It maybe a detail you didn't notice as important and I don't know and do not imagine as being possibly important. Without having your hardware on my desk (which is full with my own hardware), I have no more ideas. Sorry.
Please don't be sorry, you gave me a lot of vary valuable recommendations and my project is almost completed besides battery definition for required 1 year operation.
MSP430F2002 is mainly in LPM4 (super mode, nA consumption) and wakes up upon button interrupt, then it counts down till next sleep at the same time running timer. I cannot use crystal per mechanical requirements, however for other applications it is quite attractive.
I can send hardware (will be less on my bench) which has following connections:
pin 1 - VDD, 1uF to ground,
pins 2,3,9 - switch buttons in in parallel with 1 uF to ground,
pin 4 - NC (timer out),
pins 5,6,7,8 - NC (outputs),
pin 10 - 47k to VDD,
pin 11 - NC,
pins 12,13 - NC (outputs),
pin 14 - GND
After programming I measure voltage drop on 10 Ohm resistor in VDD path.
This isn't really much. When MSP wakes from LPM, there is a sudden change in current consumption which may drain the capacitor instantly. On 1µF, 1mA will drain it by 1V within 1ms. And the supply will possibly not be able to ramp up again fast enough.Igor Radutnuy said:pin 1 - VDD, 1uF to ground,
Pullup resistors? What about leakage currents of the capacitors? usually, 100nF ceramic ones are good enough.Igor Radutnuy said:pins 2,3,9 - switch buttons in in parallel with 1 uF to ground,
How?Igor Radutnuy said:After programming I measure voltage drop on 10 Ohm resistor in VDD path.
Well, if you can't get the current smaller, make the battery bigger :) Just a joke.Igor Radutnuy said:my project is almost completed besides battery definition for required 1 year operation.
Well, one yerar is (rounded up) 9000 hours of operation. That means a plain vanilla 1800mA AA (or a good AAA) battery is good for one year at an average current of 200µA.
Never had interrupt wake up problem with 1uF on VDD for MSP430F1101, 2001, 2002 powered by various Li cells.
Internal pull up resistors with ceramic 1 uF capacitors work well - with my setup I cannot measure any leakage current in LPM4 mode.
After programming I disconnect test board from FET debugger and measure voltage drop while powering from coin cell.
I like bigger batteries myself, however coin cell is must for this project.
What about using alkaline zinc air batteries? Twice the punch for the same size. I use dthem once for my RTC modules for the C64. I got quesitons about how to replace it, many years after I stopped manufacturing these modules. Well, I used a germanium diode (its leakage current) as charge regulator when the supply was on. Zinc-air batteries are partially rechargable too.Igor Radutnuy said:coin cell is must for this project
Well, LI cells are low impedance enough to have no problems with a sudden current increase, simple alcaline con cells might. However, you're right that 1x and 2x family with their VCC-driven core migh tnot need so much capacitance. 5x family with its internal core voltage regulator requires at least 4,7µF as the very minimum.Igor Radutnuy said:Never had interrupt wake up problem with 1uF on VDD for MSP430F1101, 2001, 2002 powered by various Li cells.
Well, it would be nice to know where the current actually flows. Maybe you're looking into the completely wrong direction. You could try a bare MSP with nothing else on the board (except the cap on the supply). No resistors, no other caps, nothing else.Igor Radutnuy said:After programming I disconnect test board from FET debugger and measure voltage drop while powering from coin cell
That’s a good point, Victor. This might indeed be the reason. On 5x family, VLO has no fault flag and switching to it is always successful. But on 2x family, VLO is just a “poor man’s XT1 crystal” and fault handling is the same as for the real XT1 (and since using XT1 is the default, there is a default-fault at startup)
**Attention** This is a public forum