I am using a MSP4302553 in battery power device that generates quite a bit of static. We have some weak grounding that prevent any ESD.
The issue seems that as static builds up the VLO that we use for waking up during sleep becomes unstable can lock up entirely until we manual discharge the static build up.
I have removed all the application code and just use the the use sleep to toggle a LED and still see the flashing become unstable and even lock up all together.
It seems that the VLO is highly sensitive to static build up.
I am looking for any suggestions( aside from putting a stronger ground on to dissipate the static) or existing documentation about this issue. Either in software or layout. Is there another processor in the family that might be less sensitive to this issue?
Is there anything else that I should try to further isolate this issue?