Hi
I am using IAR Embedded Workbench to program MSP430F5438A . I am trying to burn the UserExperience Demo program into the MSP430. The program is building fine without any errors any or warnings. Then i am using the Download and Debug option to burn the program into the uC in-circuit with the MSP-FET430UIF. In the console it is coming Download Complete but it does not seem that the program is not being flashed. I am running my program in Emulator Mode. I dont know what the problem is ....
How to solve this ?
Also, If anyone can provide the instructions that i should follow to burn code into MSP430 ( I have read the User Guide for both MSp430F5438A and IAR Embedded Worbench). May be i am missing something..............