I think that MSP430G2553 supports 32.768Hz oscillator logic input to LFXT1 with the setting of LFXT1Sx=11 & OSCOFF=0.
In this case, I would like to confirm the DC characteristics for clock logic input. Is it the same specification as schmitt-trigger input, port px?
Also, if duty and DC characteristics meets G2553's requirement, can we use not only trapezoidal wave but sinusoidal input as external clock source to LFXT1?
Best regards,
Masa