This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems with MSP430F5438A USB BSL Firmware update

Other Parts Discussed in Thread: MSP430F5438A

We are currently having an urgent issue with the bootstrap loader in the MSP430F5438A revision F. We want to be able to download a TI-TXT file and program our device using USB. The CP2102 USB to UART bridge is used to connect to the MSP430. When attempting to use the batch file that TI gives out as an example (the test scripts in slaa535a), we receive an error that says {ee} as shown in the screenshot below.

With the script:

MODE 5xx COM1
VERBOSE
MASS_ERASE
RX_PASSWORD
RX_DATA_BLOCK BLINK_MSP430F5438A.txt
DELAY 2000
RX_DATA_BLOCK BOR.txt

After looking at the test and reset pins on a logic analyzer, it is clear that the start up sequence is not correct. It is almost as if the reset signal is inverted. Here is what it looks like:

But it should look like:

It appears that there are two other threads where people had the same problem, but they were not resolved.

Does anyone have any idea what could be going wrong?
Thank you,
Chris

**Attention** This is a public forum