Hi,
I am using CP2102 based usb2uart module to program MSP430f5435 using BSL_Scripter.exe. But I am experiencing few strange situations. I have been able to communicate between the PC and the MSP using the above module. But when i connect the same module to program the msp using cmd I am getting errors. The connections as given below:
usb2uart MSP430
TX TA0.1
RX TA0.0
DTR RST/NMI
RTS TEST
VCC VCC
GND GND.
I have just connected the things and in cmd executing the BSL_Scripter.exe filename.txt . Do i need to do anything explicitly to invoke the BSL..?? I assume just by executing the above command in cmd will invoke the BSL and dumps the code to flash memory of msp.
The snapshot of the error looks like below:
And the code in the script.txt is
MODE 543x_family COM14
MASS_ERASE
DELAY 1000
RX_PASSWORD
RX_DATA_BLOCK passb.txt
Also when i change COM14 to USB in cmd its not showing any error. Even when nothin is connected to the PC.
So can someone please identify where am i going wrong..??