This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5739 + CC3000

Hi,

Can any one help in making LED1 through LED6 to glow of "WiFi Sensor Application" that I am trying to download the application using IAR 5.51 version creating new work space and adding files from CC3000Host_driver, cc3000_SPI as libraries and CC3000_SensorApp as an executable using the option project->Download->Download Active application and it downloads but LEDS won glow as it work downloading through the build-in down loader in the original demo application package from TI.

 Thanks in advance.

**Attention** This is a public forum