This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FET-Pro430 problem IAR



Hello! 

I'm using the programator FET-pro430 and IAR software on windows7,  For the reference hardware i use a cronos ez 430 watch.

I think that i have problem with programator fet-pro430. When i was click on Download and debug, the IAR send masage:  The firmware on the TI USB FET does not match this software verison. Do you want to update the firmware?

- If i click YES: Fatal error: Failed to initialize......

-if click NO: comunication error

I read that is problem with drivers for fet-pro430, so i was try to downgrade the drivers.

When i confirm with y: updateTool.exe is not recognized as an internal or external command operable program or batch file.

Then i try with code composer studio, and it is the same. 

Then i try with crossWorks for MSP. With this program it works, i can program the device, but always asking me whether I want to Update the fet-pro430.

I'm almost giving up with these processors (all TI), becouse three months ago, everything worked normally.

Best Regards Zvonko

**Attention** This is a public forum