This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In CCS 5, I generated a class by using File=>New=>Class and called it CharQueue. Which generated two files, CharQueue.h and CharQueue.cpp. the listing of the class is below.
class CharQueue {
private:
void start_pp(); // incruments start pointer
void end_pp(); // incruments end pointer
// shoudl be private
unsigned int start; // First character in buffer
unsigned int end; // Next open Character Character in buffer
unsigned char buffer[BUFF_LEN];
public:
CharQueue(); // constructor
int enqueue(unsigned char data[], int data_length); // add string to stack
int enqueue(unsigned char); // add char to stack - overloaded
int buffer_size(); // returns true if stack is not empty
char dequeue_char(); // deque char from stack (DISABLES INTERRUPTS)
};
When i build all I get the following errors:
expected a ";"
identifier "class" is undefined
My target is MSP430FR5735. Why would I get these errors? Looking at compiler reference, it handles C++ classes.
**Attention** This is a public forum