Other Parts Discussed in Thread: MSP430G2553, MSP430F1612, MSP-FET
Every few days I start getting a 'MSP430: Error initializing emulator: No USB FET was found' when I build my projects, this problem lasts for a few more days until it spontaneously resolves itself. When this happens, Windows will report it as an unknown device with an error code of 43. I can't test building this on multiple computers or multiple launchpads at the same time. I had a revision 1.4 in the past which had the same problem.
Processor:MSP430G2553
Launchpad: MSP-EXP430G2 Rev. 1.5
CCSv5.3.0.0.00090
Windows 7 x64
Fixes attempted:
Multiple USB cables and multiple ports some with and some without hubs
Reinstalling CCSv5 with and without USB attached
Rebooting with and without USB attached
Replacing the MSP430 processor