Other Parts Discussed in Thread: MSP430F6736, MSP430F5438
I downloaded the HID Demo source and I've been trying to get it working on the MSP430F6736. I noticed that the SetSystemClock function disables the ACLK ISR. Any ideas on what I need to change to get it working? Here's the original code
static void SetSystemClock(Cpu_Frequency_t CPU_Frequency)
{
Boolean_t UseDCO;
unsigned int Ratio;
unsigned int DCODivBits;
unsigned long SystemFrequency;
volatile unsigned int Counter;
BTPSCONST Frequency_Settings_t *CPU_Settings;
/* Verify that the CPU Frequency enumerated type is valid, if it is */
/* not then we will force it to a default. */
if((CPU_Frequency != cf8MHZ_t) && (CPU_Frequency != cf16MHZ_t) && (CPU_Frequency != cf20MHZ_t) && (CPU_Frequency != cf25MHZ_t))
CPU_Frequency = cf16MHZ_t;
/* Do not allow improper settings (MSP430F5438 cannot run at 20MHz or*/
/* 25 MHz). */
if((!DetermineProcessorType()) && ((CPU_Frequency == cf20MHZ_t) || (CPU_Frequency == cf25MHZ_t)))
CPU_Frequency = cf16MHZ_t;
/* Get the CPU settings for the specified frequency. */
CPU_Settings = &Frequency_Settings[CPU_Frequency - cf8MHZ_t];
/* Configure the PMM core voltage. */
ConfigureVCore(CPU_Settings->VCORE_Level);
/* Get the ratio of the system frequency to the source clock. */
Ratio = CPU_Settings->DCO_Multiplier;
/* Use a divider of at least 2 in the FLL control loop. */
DCODivBits = FLLD__2;
/* Get the system frequency that is configured. */
SystemFrequency = HAL_GetSystemSpeed();
SystemFrequency /= 1000;
/* If the requested frequency is above 16MHz we will use DCO as the */
/* source of the system clocks, otherwise we will use DCOCLKDIV. */
if(SystemFrequency > 16000)
{
Ratio >>= 1;
UseDCO = TRUE;
}
else
{
SystemFrequency <<= 1;
UseDCO = FALSE;
}
/* While needed set next higher div level. */
while (Ratio > 512)
{
DCODivBits = DCODivBits + FLLD0;
Ratio >>= 1;
}
/* Disable the FLL. */
__bis_SR_register(SCG0);
/* Set DCO to lowest Tap. */
UCSCTL0 = 0x0000;
/* Reset FN bits. */
UCSCTL2 &= ~(0x03FF);
UCSCTL2 = (DCODivBits | (Ratio - 1));
/* Set the DCO Range. */
if(SystemFrequency <= 630)
{
/* Fsystem < 630KHz. */
UCSCTL1 = DCORSEL_0;
}
else if(SystemFrequency < 1250)
{
/* 0.63MHz < fsystem < 1.25MHz. */
UCSCTL1 = DCORSEL_1;
}
else if(SystemFrequency < 2500)
{
/* 1.25MHz < fsystem < 2.5MHz. */
UCSCTL1 = DCORSEL_2;
}
else if(SystemFrequency < 5000)
{
/* 2.5MHz < fsystem < 5MHz. */
UCSCTL1 = DCORSEL_3;
}
else if(SystemFrequency < 10000)
{
/* 5MHz < fsystem < 10MHz. */
UCSCTL1 = DCORSEL_4;
}
else if(SystemFrequency < 20000)
{
/* 10MHz < fsystem < 20MHz. */
UCSCTL1 = DCORSEL_5;
}
else if(SystemFrequency < 40000)
{
/* 20MHz < fsystem < 40MHz. */
UCSCTL1 = DCORSEL_6;
}
else
UCSCTL1 = DCORSEL_7;
/* Re-enable the FLL. */
__bic_SR_register(SCG0);
/* Loop until the DCO is stabilized. */
while(UCSCTL7 & DCOFFG)
{
/* Clear DCO Fault Flag. */
UCSCTL7 &= ~DCOFFG;
/* Clear OFIFG fault flag. */
SFRIFG1 &= ~OFIFG;
}
/* Enable the FLL control loop. */
__bic_SR_register(SCG0);
/* Based on the frequency we will use either DCO or DCOCLKDIV as the */
/* source of MCLK and SMCLK. */
if (UseDCO)
{
/* Select DCOCLK for MCLK and SMCLK. */
UCSCTL4 &= ~(SELM_7 | SELS_7);
UCSCTL4 |= (SELM__DCOCLK | SELS__DCOCLK);
}
else
{
/* Select DCOCLKDIV for MCLK and SMCLK. */
UCSCTL4 &= ~(SELM_7 | SELS_7);
UCSCTL4 |= (SELM__DCOCLKDIV | SELS__DCOCLKDIV);
}
/* Delay the appropriate amount of cycles for the clock to settle. */
Counter = Ratio * 32;
while (Counter--)
__delay_cycles(30);
}