This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the maximum data transmiot rate

I need to transmit data over the air  with a rate of 200KHz.(sample an ADC and transmit the sampled data).

is it even possible with  CC430F6137 (433MHz or 915MHz)? what is the max transmit rate possible?

  • The sensitivity tables give  ahint: for 433MHz, they only have a 250kBd row, for 868 and 915MHz, there's a 500kBd row.
    The users guide also tells "Programmable data rate from 0.8 kBaud to 500 kBaud" for the "CC1101-based radio module"

    For 200ksps, you'd need at least 1.6MBd (8 bit data) or even 2.4MBd (12 bit), not counting the overhead for the package frame. On a serial port (with start and stop bit), you'd at least need 2MBd, which is twice as much as the serial UART allows.

    You may try to reduce your data by some sort of compression. e,g a bitstream where each bits tells '+1' or '-1' relative to the last value. Or two bit per value, stating +1, -1, +-0 or an absolute value following the two bits. This allows a shortcut for larger jumps.

**Attention** This is a public forum