Hello!
I am currently working on a hardware design for an MSP430F5506. I however have never done a design for an MSP430 before and I am not really sure what pins I need and so on. Below is a schematic picture of the initial design I recently started:
I have just connected a JTAG interface and imported the UART interface from my RS-485 transciever. I have no need for any USB connection as I will use the JTAG interface for programming and so on. I will also implement a SPI interface to a CC1125 transciever alongside the UART interface. I am wondering about such pins as Vcore? I am not sure if I need it or not? And the Vusb, V18, DP, DM, PUR and Vbus connections I can just leave unconnected then?