I'm doing a project IR control project. I'm controlling the LED with a transistor. I've had no luck so far getting the forward voltage and current for the IR LED from the ebay seller (lesson learned, ask for specs before buying.) So I played it safe and connected a 150 ohm resistor but it appears that the LED is not getting enough current to do its job. I've done a resistor calculation based on what some people said that an typical IR LED runs at 100mA and an forward voltage of 1.2v and came up with 22 ohms. Is this a good estimate?