This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430F5529 Experimenter Board's ADC value display on LCD

Other Parts Discussed in Thread: MSP430F5529

I am developing an application where i can take analog readings on port 7.0 of MSP430F5529 (A12 channel of LCD), I am using variable resistance to take reading on port 7.0 (Channel A12). on board ADC12, Using the Internal Reference, The ADC12 uses the internal 2.5V reference and performs a single conversion on channel A12. The conversion results are stored in ADC12MEM0. Test by applying a voltage to channel A12, then setting and running to a break point at the "__no_operation()" instruction. I want sampled values to be displayed on onboard LCD.

for this i am using code 


#include <msp430f5529.h>

void main(void)
{
  volatile unsigned int i;


  WDTCTL = WDTPW+WDTHOLD;                // Stop watchdog timer


  P7SEL |= 0x01;                                                // Enable A/D channel A0


  REFCTL0 &= ~REFMSTR;                              // Reset REFMSTR to hand over control to
                                                                               // ADC12_A ref control registers


  ADC12CTL0 = ADC12ON+ADC12SHT02+ADC12REFON+ADC12REF2_5V;
                                                                              // Turn on ADC12, Sampling time
                                                                              // On Reference Generator and set to
                                                                              // 2.5V


  ADC12CTL1 = ADC12SHP;                          // Use sampling timer


  ADC12MCTL0 = ADC12SREF_1;                // Vr+=Vref+ and Vr-=AVss

  for ( i=0; i<0x30000; i++);                              // Delay for reference start-up
 
  ADC12CTL0 |= ADC12ENC;                       // Enable conversions

  while (1)
  {
    ADC12CTL0 |= ADC12SC;                         // Start conversion
    while (!(ADC12IFG & BIT0));
    __no_operation();                                        // SET BREAKPOINT HERE

  }
}

Now i want further Program such that whatever value ADC takes it should display it on onboard LCD and stores onto the Register ADC12MEM0 as well. Further ADC12_A related details can be found out on SLAU208K document on Page No. 722. I stuck in the programming where i am not able to display the Variable resistance (Voltage Levels) value on LCD. Can anyone write further Program with Function to display Voltage level / Equivalent decimal or HEX value onto the LCD for single conversion ?

**Attention** This is a public forum