Other Parts Discussed in Thread: MSP430G2452, MSP430WARE
Hi,
I am having a problem with my code, I simply want to set a flag to ensure that the ADC interrupt is working but it doesn't seem to be working.
Here is my code...
#include <msp430g2452.h>
void initAdc();
volatile char flag = 0;
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1DIR |= BIT6;
P1OUT &= ~BIT6;
initAdc();
__bis_SR_register(GIE);
while(1){
if(flag == 1){
P1OUT |= BIT6;
}else{
P1OUT &= ~BIT6;
}
}
return 0;
}
void initAdc(){
ADC10CTL1 = CONSEQ_2 + ADC10DIV_3; //Channel A0 for conversion, ADC10OSC clock used for sampling, repeat single channel
ADC10CTL0 = ADC10SHT_2 + MSC + ADC10ON + ADC10IE + ADC10SC + ENC; //sample and hold time every 16 clocks, Multiple sample conversion, turn on ADC, enable interrupts for ADC, every 16 clock cycles take a sample
ADC10DTC1 |= 0x01; //Number of transers in each block
ADC10AE0 |= 0x01; //Enables the corresponding pins for analog inputs
}
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR(void) {
flag = 1;
}