This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 Series Development Board

Is there a development board TI sells that I can use to experiment with multiple series of MSP430s? I saw the MSP430 experimenter board, and it looks like processors can be swapped in and out of the board, but it looks like the board is designed very tightly with the MSP430F5xxx series. Is that right? If it is, are there any options available, such as a breakout board, where the MSP430 processor can be swapped out as needed?

**Attention** This is a public forum