Hi,
I am new to code composer studio and msp43016F1611.
I have a code written by my client where there is a File called Interupt.c and have the following code.
#include <msp430x16x.h>
extern interrupt void Timer_A0_Handler(void);
TIMERA0_ISR(Timer_A0_Handler)
extern interrupt void Timer_A12_Handler(void);
TIMERA1_ISR(Timer_A12_Handler)
extern interrupt void Port2_Handler(void);
PORT2_ISR(Port2_Handler)
extern __interrupt void I2C_Handler(void);
USART0TX_ISR(I2C_Handler)
extern interrupt void ADC_Handler(void);
ADC12_ISR(ADC_Handler)
extern interrupt void NMI_Handler(void);
NMI_ISR(NMI_Handler)
extern interrupt void Comparator_Handler(void);
COMPARATORA_ISR(Comparator_Handler)
extern interrupt void UARTTX_Handler(void); //BT #1481864546
USART1TX_ISR(UARTTX_Handler)
in #include <msp430x16x.h> i could see all the #defined used in thsi file (e.g, TIMERA0_ISR,.......USART1TX_ISR,COMPARATORA_ISR) all are under commented section and so the workspace is not compiling.
Could someone suggest whether is it advisable to use TIMERA0_VECTOR instead of TIMERA0_ISR (like wise for all others)
Thanks and Regards,
Aarthi