This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F5510 HID Keyboard with UART Function

Hi Everyone,

I download and used the example code from TI about SLAA514 ( HID Keyboard ).

I add UART Initial and interrupt on main like below .

and i have set GIE, but the UART INT not work when i send data from PC UART.

I want change the example coed frome USB Keyboard to USB+BT(UART Interface) Keyobard.

but i don't know how to add UART function into this code.

Please give me some idel.

.............

static void Init_Uart(void)
{
P4SEL = BIT4+BIT5+BIT3; // P3.4,5 = USCI_A0 TXD/RXD
UCA1CTL1 |= UCSWRST; // **Put state machine in reset**
UCA1CTL1 |= UCSSEL_1; // CLK = ACLK
UCA1BR0 = 0x03; // 32kHz/9600=3.41 (see User's Guide)
UCA1BR1 = 0x00; //
UCA1MCTL = UCBRS_3+UCBRF_0; // Modulation UCBRSx=3, UCBRFx=0
UCA1CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA1IE |= UCRXIE; // Enable USCI_A0 RX interrupt
}

........

#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR(void)
{
switch(__even_in_range(UCA1IV,4))
{
case 0:break; // Vector 0 - no interrupt
case 2: // Vector 2 - RXIFG
while (!(UCA1IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
UCA1TXBUF = UCA1RXBUF; // TX -> RXed character
break;
case 4:break; // Vector 4 - TXIFG
default: break;
}
}

**Attention** This is a public forum