Other Parts Discussed in Thread: MSP430G2553
I am using the M430G2553 chip and trying to do a PWM program to control a servo. I have the script running and it works good except I can see on my scope that every few seconds I get a signal that is at full voltage for the duration of the idle time. It only happens very suddenly and at random and only for 1 signal duration. This is causing my servo to jitter. I have isolated it to the program because when the pot is fully turned to the 10k resistance (the ADC10MEM reads 0x03FF) there is no jitter at all. When I move anything lower than this the jitteryness happens. I think it has something to do with the ACD10MEM having problems because when I remove this and hard code a value in it's place, everything works fine. If I put a 1k resistor in place of the pot it still jitters so it does not have anything to do with a bad pot. Do you know why this is happening? Code is below:
#include "msp430g2553.h" // make sure you change the header to suit your particular device.
/*
* Vcc To POT
* P1.1 From POT
* P1.2 To Servo
*/
#define MCU_CLOCK 1000000
#define PWM_FREQUENCY 46 // In Hertz, ideally 50Hz.
unsigned int PWM_Period = (MCU_CLOCK / PWM_FREQUENCY); // PWM Period
void main(void) {
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P1DIR |= 0x0C; // P1.2 and P1.3 output
P1SEL |= 0x0C; // P1.2 and P1.3 TA1/2 options
TACCTL1 = OUTMOD_7; // TACCR1 reset/set
TACTL = TASSEL_2 + MC_1; // SMCLK, upmode - SETUPS TIMER
TACCR0 = PWM_Period-1; // PWM Period - NUMBER TO COUNT TO
//ADC10CTL0 = ADC10SHT_2 + ADC10ON + ADC10IE; // ADC10ON, interrupt enabled
ADC10CTL0 = SREF0 + ADC10SHT_2 + ADC10ON + REFON + REF2_5V + ADC10SR;
ADC10CTL1 = INCH_1; // input A1 ADC10AE0 |= 0x02; // PA.1 ADC option select
for (;;){
ADC10CTL0 |= ENC + ADC10SC;
while (ADC10CTL1 & ADC10BUSY);
TACCR1 = ADC10MEM;
}
}