Other Parts Discussed in Thread: MSP430G2203
Dear Sirs
I have to use the QFN version of the MSP430G2203 micro.
It has an AVCC pin.
What is the AVCC range ?
Where do I have to connect it?
Thank you in advance
Best Regards
Andrea Sorio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2203
Dear Sirs
I have to use the QFN version of the MSP430G2203 micro.
It has an AVCC pin.
What is the AVCC range ?
Where do I have to connect it?
Thank you in advance
Best Regards
Andrea Sorio
See the datasheet. Since AVCC and DVCC are connected through clamp diodes, AVCC ust not differ from DVCC more than the diode voltage.Andrea Sorio said:What is the AVCC range ?
The main reason for a separate pin is that you can apply a filtered version of DVCC (without digital ripples) to it. A common approach is to connect AVCC to DVCC with a 10 ohms series resistor and put a separate deblocking capacitor on it. If ADC precision isn't an issue, you can just connect the two.
Similar for DVSS. To avoid currents on DVSS lifting the GND level for the analog parts, it is recommended that teh analog circuitry has its own GND (wher enot operating currents flow) and which is connected with the digital GND right at the supply. Again, if precision is unimportant, you can just connect the two.
**Attention** This is a public forum