Other Parts Discussed in Thread: MSP430G2313, TCA6507, MSP430G2452, LP2951, SN74AHC595, TLC6C598
I am looking at using an MSP430G2313 Value Line uC + LCD or LED driver (I2C or SPI).
For example, the display I am looking at is a ChromeLED P/N: SDTA28R2W
I have tested the code using the MSP - EXP430FG4618, using LCD display. The issue is that the low cost 4 series MSP's are 8MHz CPU (no DCO calibration) , and I'm in a hurry (like 16MHz :), desire better accuracy with the DCO, and have a target budget cost for the end product.
I found the ST-micro LED controller P/N: STED316S
I want to find a TI replacement for the above part, but designed for 3.3V use with the MSP.
I know there is more than one way to skin a cat. This cat wants small code size, low cost, low pin-count, and all that stuff :)
Can someone suggest a TI part that can get the job done? I prefer to use the LED display because of the working environment for the end product, but to include all options an LCD driver my be appropriate?