This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779PZ and Spy-bi-wire programming

Other Parts Discussed in Thread: MSP430F6779

Are there any special conditions required for the spy-bi-wire interface to work in a MSP430F6779IPZ? There is power (3.5V, provided by the programmer) at the AVCC and DVCC pins and I can see that the VCORE pin is at 1.5V but the Elprotronic MSP430 programmer ver 3.1 reports that the MCU is not responding. I have checked that the RESET pin and the TEST pins are connected properly.

Does anyone have any ideas or suggestions?

Thanks,

Robert

  • Hi Robert,

    Does your schematic follow the recommended interface in the MSP430 Hardware Tools User's Guide (Rev. M)?  http://www.ti.com/litv/pdf/slau278m

     

     

        Best,

            Rick Nardone

  • Hi Rick,

    Thank you for taking time to respond and for going that "extra yard" to attach connection schematics and link to relevant document. I have gone through the document and I can confirm that my PCB is compliant and in particular, I am using a 1nF capacitor in the reset circuit. The difference between the schematics and my environment is that I am using a four-pin header and I am using an MSP430Launch pad as programmer. (This worked well with MSP430F2xx devices with Spy-By-Wire inferfaces.)

    I noticed that the LCDCAP pin(pin 47) was not connected on my PCB and I have now grounded this, without success - I still can't communicate with the 6779. In the event I damaged the MCU during the assembly of the PCB, I have request another couple of samples from TI and I'll post here the results when I receive the samples. Unfortunately, this particular device is not commercially available yet and it was an almost perfect match for my intended application!

    EDIT: I have swapped the MSP430LaunchPad with a MSP-FET430UIF using the connections shown in the document and I am pleased to advise that I now have communications with the MSP430F6779. By the way, the schematics attached in your post is missing a connection between pin-8 of the JTAG connector and pin-7 of the same connector. I soldered a 330 Ohm resistor between pin-7 and pin-8 and a wire from pin-8 to the TEST/SBWTCK pin of the MCU.

    Would you happen to know why the MSP430LaunchPad does not work with the 6779? Firmware upgrade required to handle MSP430F6xx devices?

    Regards,

    Robert

  • Hi Robert,

       Glad to hear that you are moving forward! 

       See Table 1-1 from the MSP430 Hardware User's Guide for the answer to  your last questions:

     

     

       Have a great weekend,

              - Rick

        

  • Hi Rick,

    Thanks once again for your prompt reply and for pasting the table instead of just referencing the source document!

    From my understanding of the Spy-By-Wire there is nothing in the SBIW protocol that requires hardcoding in an implementation to support a MSP430F family; I guess that this probably means that the firmware of the programmer in the MSP430LaunchPad has some hardcoding that prevents its use with the MSP430F6xx devices.

    Thanks once again.

    Regards,

    Robert

**Attention** This is a public forum