This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 GANG programmer works interactively, but cannot get standalone to work.

I have successfully used the MSP430 GANG programmer to burn various embedded chips via a standard JTAG connection.  When using "interactive" mode, it works perfectly.

Unfortunately, I have yet to get the "standalone" mode to work (i.e. GANG programmer NOT connected to a PC).  I believe I have followed the documentation (SLAU358) on how to do this, but still no luck.  Here are my steps using the software provided with the device:

1) After configuring everythinig for interactive mode (and testing) I "Save As".  This generates an mspgangimage file and an mspgangbin file.

2) I then go to "From Image File" and select my mspgangimage file that was just created.  ("Config From Image" checkbox is selected)

3) I do one "Go (F9)" from UI.  This burns my target(s) perfectly.  On the LCD of the Gang programmer, I see that everything works too and that the CRC is the same as reported in the UI.

So far so good, but now, I want to go "Standalone".  (The LCD is "locked" until I select "Standalone" from the UI)

4) Using the GANG programmer buttons, I Select the image I just created (Image 001)

5) After hitting "Go" I get the following error(s)  "2 Init Target  Used wrong MCU  Failed Err 32"

So, I think there is something I'm missing here.

Also, a secondary problem: I have also attempted to put my mspgangimage and mspgangbin files on an SD card and put that in the GANG programmer.  Unfortunately, I get an Err 45 (SD timeout) message when I do that.  Perhaps this problem is related to the first one ... or perhaps it's a different issue.

Please help.

Thanks!

Thaddeus

 

**Attention** This is a public forum