Hi,
I am using windows 7 (64-bit).
When I try download a program into my msp430, I am getting de following error message
Could not find MSP-FET430UIF on specified COM port
In de options (IAR embedded workbench) I choose Debugger -> FET Debugger -> Connection texas instrument USB-if -> automatic
If I try to select a port I see HID0021:COM4 (already in use). I can't select port because it is in use.
If a disconnect the device, the message HID0021:COM4 disappears.
It seems that the port can't be selected because it is reserved for it self.
How can I solve this problem ?
What can I for further investigation