This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with printing to the console

Other Parts Discussed in Thread: MSP430F247

Hi,

I'm using CCS5 with a MSP430F247. I need outputs to help with debugging and monitoring.

I set up the 'Variant' field. Enabled CI\O support and increased stack and heap sizes.

My code is as follows:  (by the way, how come there are no <code> tags?)

#include <msp430.h>
#include <stdio.h>

int main(void) {
    WDTCTL = WDTPW | WDTHOLD;    // Stop watchdog timer

    putc ('a', stderr);

    return 0;
}

This is just a test project so I could rely on the console in the future.

When I run the run this, the character 'a' gets printed to the CIO console, but I get "MSP430: Trouble Writing Memory Block at 0x1240 on Page 0 of Length 0xa: Could not write device memory" on the project console and the debugger gets stuck at function C$$IO$$(). The memory address 0x1240 points to the beginning of _CIOBUF_.

If I use fprintf(stderr, "string"), it will also print and give the same error and get stuck.

if I use the regular printf() or fprintf() with stdout, nothing happens (even though in the wiki pages it says it should print to the console).

I would highly appreciate ideas as to how to print safely to the console.

Thanks.

**Attention** This is a public forum