This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need USB Mass Storage Drivers for MSP430F5529 EXP. Board

Hello,

can somebody tell me where I can download the Mass Storage drivers for the MSP-EXP430F5529? Windows 7 and 8 download the driver automaticly over the internet. But I have a Windows XP System without the possibilty to connect to the internet. Is there any chance to get the driver somewhere else because I can't find it online?

Thanks in advance!

  • Marcel Wagner said:
    can somebody tell me where I can download the Mass Storage drivers for the MSP-EXP430F5529?

    Starting with Windows 2000, Windows operating systems contain native support for devices that are compliant with the USB Mass Storage Class Specification. If the USB bus driver enumerates a mass-storage-class-compliant device on a computer running Windows, it automatically loads the USB storage port driver (Usbstor.sys) for that device. So third party generic drivers are not needed.

    Maybe I am missing something?!?

    Regards,

    Mo.

**Attention** This is a public forum