Other Parts Discussed in Thread: MSP430L092
Hello,
Simply put, I'm just trying to load some example code onto the MSP430L092 using the MSP-TS430L092 evaluation kit. It should be quite straight forward and yet I haven't been able to get it going. I'm using IAR Embedded, created a new project using the settings given in the fold out pamphlet and have set all the jumpers (JP1 both 1 & 2, JP2 on the active cable PCB as well as JP1, JP2 and JP3 on the target socket) which is all connected to my PC with the MSP-FET430UIF. When I try to download the code to the target board I get:
The MSP430L092 is in the correct orientation in the socket. LEDs blink three times during initial power up of the FET430UIF so I believe the boost circuit is operating as it should.
Can someone shed some light as to what's going wrong here? I'm by no means an expert in this realm, any help would be greatly appreciated!
Here's a photo of my setup:
Thanks