Hi everyone!
I have just received my PCB but I am having problems programming my MSP430f5507 MCU. I have a MSP-FET430UIF debugger and I use CCS v5 for the coding and I ahve tried using CCS to debug but also the FET-PRO430 programming software. Neither of these works and I cant program my MSP430f5507.
Below is a picture of the schematic connections of the JTAG interface. I use the 2-wire spy-by-wire connection but I cannot upload code into my MSP430f5507. The firmware of the FET debugger is 3.02.05.004. The card powers up like it should but I just cant initialize JTAG communication with my MSP. Can someone help me pls? The J1 connector is simply so I can choose if the processor should be powered from the battery or the debugger.
/Mikael