This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Fraunchpad (MSP430FR5739) + CC1120EMK + SmartRF

Other Parts Discussed in Thread: MSP430FR5739, CC1120

Hello,

Is it possible to configure the CC1120 connected to my MSP430FR5739 by directly using SmartRF? At the moment SmartRF is able to detect my MSP430 but it considers it an unknown device. Do I need to load up a special program to do so?

Is the only way to do it manually? (using SmartRF to calculate the register values and then using a MSP430 code to configure the CC1120). Are there any code examples to do so? I have looked but have not found anything.

I also own a CC1120 Performance Line Development Kit and even though the board has its own program, I can connect it to the PC and easily use smart RF to configure the radio communication parameters. I want to be able to do this from my FR5749.

Thanks a lot in advance.

**Attention** This is a public forum