Other Parts Discussed in Thread: MSP-EXP430FR5739, ENERGIA, MSP430F5510
Hi folks,
I am a bit astonished about the Linux policy of TI.
On the one hand it will be pronounced that Linux is supported for the Launchpads (indirectly), on the other hand it seems that it does not work.
Or I am to unhandy to deal with it. I hope I can clarify this here and I do this on the right way.
First of all I bought 4 Launchpads over the time, because I really like the less expensive and well equipped devices:
http://www.ti.com/tool/MSP-EXP430G2
http://www.ti.com/tool/msp-exp430fr5739
http://www.ti.com/tool/ek-lm4f120xl (Stellaris)
http://www.ti.com/tool/launchxl-f28027 (C2000 Piccolo)
and the fancy watch http://www.ti.com/tool/ez430-chronos.
OK, the Stellaris and C2000 Piccolo are no MSP430, but I think the case is the same.
All of them are advised as programmable with CCS5. And the Code Composer Studio exists in Windows and Linux version. So I thought the LaunchPads are programmable under Linux with CCS5.
On Windows I can program the MSP-EXP430G2, on Linux I can't. The error "Error initializing emulator: No USB FET was found" appears. With the MSP-EXP430FR5739 the same problem.
The point is, it is a known issure:
JohnS (TI Employee):
"Per,
The LaunchPad is not supported on Linux at this time.
John"
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/171173/688729.aspx#688729
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/221603.aspx
So, why is that Link broken:
X is Programmable with CCS5-->CCS5 exists for Linux-->X is programmable on Linux? ;)
At least the EXP430G2 is programmable on Linux:
http://hackaday.com/2010/08/11/how-to-launchpad-programming-with-linux/
http://losinggeneration.homelinux.org/2010/07/02/msp430-launchpad-on-linux/
But it bypasses the CCS5. Why is it not possible to include the tools (MSPGCC & MSPDEBUG) in the tool chain of CCS5? Or is it?
What is with the other LaunchPads, are there solutions for programming on Linux?
Or what else can I do to program MSP430-Controller with CCS5 on Linux? Even without a LaunchPad?
___
Similar problem with other tools. The tool FRAM_GUI is a Windows binary. But the source is open. Exists a compilation for Linux already?
Thanks to all
Fabian Hoemcke
Berlin
Code Composer Studio Version: 5.4.0.00091
- installed as user
- install_drivers.sh executed as sudo
Ubuntu 13.04 (32bit)