This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM430-F47197 3 ph e-meters and two tmdsplckitV3 PLC modems



I recently acquired two EVM430-F47197 3 ph e-meters which I hope to connect to two tmdsplckitV3 PLC modems.  I have had some success with the modems but am having a problem connecting to the EVM430-F47197.

After powering the an e-meter it seems to be operating normally.  It cycles through the readings.  The Application Report I have, SLAA409A has a V4.0 calibration.exe application.  Using this software I have tried to communicate to the unit but after pressing the green Comms button the meter status page appears but does not respond.  I am running Windows 7 on this PC and have tried changing different compatibility modes on calibrator.exe.  I'm hoping someone has had this issue and can help me.
Thanks
GM

**Attention** This is a public forum