This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg how to drive realy using msp430/stellaris

Hi,

I  am working with msp430 , I have relay board( 230v,5A relay  ,5v coil really connected with BC 547) , will 3.3v of  MSP430 gpio pin  will drive BC547 to switch on/off  realy ?

Regards,

Tamil

  • tamil vanan said:
    will 3.3v of  MSP430 gpio pin  will drive BC547 to switch on/off  realy ?

    Yes GPIO pin current sourcing capability is more than sufficient to open BC547 transistor. Make sure series resistor between gpio and base of transistor is in range 1k .. 470ohm and you will be fine.

**Attention** This is a public forum