Hello
I have ez430 chronos watch and microprocessor CC430F6137 with antena. I want connect watch with CC430 "per to per" 868MHz. Do you have any examples? :)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I have ez430 chronos watch and microprocessor CC430F6137 with antena. I want connect watch with CC430 "per to per" 868MHz. Do you have any examples? :)
Hi,
there are examples available
http://e2e.ti.com/group/universityprogram/educators/w/wiki/2043.msp430-teaching-rom.aspx
http://processors.wiki.ti.com/index.php/EZ430-Chronos
Regards,
Maciej
hej Maciej a możesz mi powiedzieć na co zwrócić uwagę przy zabawie z Simpliciti? Szczerze to mało jest informacji w necie i mało przykładów aby zacząć zabawę tak jak z AVR.
pozdrawiam
Thomas TMEA said:hej Maciej a możesz mi powiedzieć na co zwrócić uwagę przy zabawie z Simpliciti? Szczerze to mało jest informacji w necie i mało przykładów aby zacząć zabawę tak jak z AVR.
I can, but in English. This is international forum and the idea behind it is to create knowledge database that can be accessible for as many people as possible.
I would start with the teaching ROM because it is prepared for students (they often have no idea what is going on). You can look into Chronos watch source or try to understand pure http://www.ti.com/simpliciti source code. In general you have plenty to learn from from the links I gave you. e2e is also full of useful information on SimpliciTI.
Finally you can find SimpliciTI on the CC430 – Practical Modifications application note by Lisa Taubensee (http://www.ti.com/lit/an/swra321/swra321.pdf)
Regards,
Maciej
**Attention** This is a public forum