Other Parts Discussed in Thread: CC430F5137, MSP430WARE
so I've RTC_A setup awesomely in calendar mode with backup battery and all & it's working great, up until I noticed some weird behaviour when it comes to month changes.
In my code I've integrated time.h to as its use is necessary throughout the rest of the code. This was achieved by having code that converted the MSP "Calendar" data type into the "struct tm" data type. I noticed the following trend yesterday
| Date set (dd/mm) | Date after midnight |
| 31/01 | 01/02 |
| 28/02 | 01/03 |
| 31/03 | 01/04 |
| 30/04 | 01/05 |
| 31/05 | 02/06 |
| 30/06 | 01/07 |
| 31/07 | 02/08 |
| 31/08 | 01/09 |
| 30/09 | 01/10 |
| 31/10 | 02/11 |
| 30/11 | 01/12 |
| 31/12 | 02/01 |
Anyone noticed anything like this before?