This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resonator characteristics for USB applications

Other Parts Discussed in Thread: MSP430F6638

Hello,

It is possible to use a 4MHz resonator as XT2 clock for USB applications in the MSP430f6638.

What should be the minimum characteristics of this resonator?

Regards,

Raul.

  • From slau208 MSP430x5xx and MSP430x6xx Family User's Guide

    For crystal operation, a 4 MHz or higher crystal is required. For crystal bypass mode of operation, 1.5 MHz is the lowest external clock input possible for CLKSEL.

    Basically, you can use any XT2 CLK that will be inside USB spec tolerance +/- 0.25% (2500 ppm) for full-speed bus. If you want to use USB BSL than XT2 CLK must be 4, 8, 12 or 24 MHz. Here is my USB PLL configurator...

    http://forum.43oh.com/topic/3904-usb-pll-configurator

**Attention** This is a public forum