This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Absolute Maximum Ratings

MSP430F677, its data sheet show as below,

I connect DVCC (3.3V) to DVCC pin and connect 3.6V-battery +/-10% (3.96V) to AUXVCC1 pin.

     1. What is the maximum voltage from the table above that I should check for AUXVCC3 pin.

     2. If AUXVCC3 pin should be in the range of -0.3 V to VCC +0.3V, and I try to connect it. MCU will fail ?

**Attention** This is a public forum