Other Parts Discussed in Thread: MSP430F2132, MSP430WARE
Hello,
i'm wondering when the two ISR are triggered:
USCIAB0TX_VECTOR
USCIAB0RX_VECTOR
Couldn't find any Information about that.
Thank you.
Its about that example of MSP430Ware for MSP430F2132 msp430x21x2_uscib0_i2c_11, this is the I2C Slave Code. The Slave is transmitting 5 Bytes.
#include <msp430.h>
unsigned char *PTxData;
volatile unsigned char TXByteCtr;
const unsigned char TxData[] =
{
0x11,
0x22,
0x33,
0x44,
0x55
};
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3SEL |= 0x06; // Assign I2C pins to USCI_B0
UCB0CTL1 |= UCSWRST; // Enable SW reset
UCB0CTL0 = UCMODE_3 + UCSYNC; // I2C Slave, synchronous mode
UCB0I2COA = 0x48; // Own Address is 048h
UCB0CTL1 &= ~UCSWRST; // Clear SW reset, resume operation
UCB0I2CIE |= UCSTPIE + UCSTTIE; // Enable STT and STP interrupt
IE2 |= UCB0TXIE; // Enable TX interrupt
while (1)
{
PTxData = (unsigned char *)TxData;
TXByteCtr = 0;
__bis_SR_register(CPUOFF + GIE);
__no_operation();
}
}
#pragma vector = USCIAB0TX_VECTOR
__interrupt void USCIAB0TX_ISR(void)
{
UCB0TXBUF = *PTxData++; // Transmit data at address PTxData
TXByteCtr++; // Increment TX byte counter
}
#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCIAB0RX_ISR(void)
{
UCB0STAT &= ~(UCSTPIFG + UCSTTIFG);
if (TXByteCtr)
__bic_SR_register_on_exit(CPUOFF);
}