This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5969 - IP Encapsulation

Hi,

I am having problem developing a simple code for the IP Encapsulation. I use MSP430FR5969 Wolverine, MSP-FET430UIF as development kit and board MSP-TS430RGZ48C.
Here is my code:

#include <msp430.h>

#pragma DATA_SECTION (protectedVar, ".ipArea");
#pragma DATA_ALIGN (protectedVar, 1); // reserve one byte for each variable
unsigned char protectedVar[4];

#pragma CODE_SECTION (ipAccess, ".ipAreaC");
void ipAccess()
{
  unsigned char c;
  c= protectedVar[0];
  c = c+1;
  protectedVar[1] = c;
}

int main(void)
{
  WDTCTL = WDTPW | WDTHOLD;                 // Stop WDT

  P1DIR |= BIT0;                            // Configure P1.0 for LED

  // Configure MPU
  MPUCTL0 = MPUPW | MPUSEGIE | MPUENA;                          // Write PWD to access MPU registers

  MPUIPSEGB1 = 0x0440;                        // B1 = 0x4400; B2 = 0x4600
  MPUIPSEGB2 = 0x0460;                        // Borders are assigned to IP Encapsulation segments
  MPUIPC0 = MPUIPENA | MPUIPLOCK;             // IP Encapsulation enabled ;

  ipAccess();
  protectedVar[0] = 128;

  LPM3;
}

// Sys NMI vector
#pragma vector = SYSNMI_VECTOR
__interrupt void SYSNMI_ISR(void)
{
    switch(__even_in_range(SYSSNIV,0x18))
    {
    case 0x00: break;
    case 0x02: break;
    case 0x04: break;
    case 0x06: break;
    case 0x08:                              // MPUSEGPIFG Encapsulated IP Violation
      P1OUT=BIT0;
      MPUCTL1 &= ~MPUSEG2IFG;                // Clear violation interrupt flag
      __bic_SR_register_on_exit(LPM3_bits);     // Exit LPM3
      break;
    case 0x0A: break;
    case 0x0C: break;                       // MPUSEG1IFG
    case 0x0E: break;  
    case 0x10: break;                       // MPUSEG3IFG
    case 0x12: break;
    case 0x14: break;
    case 0x16: break;
    case 0x18: break;
    default: break;
    }
}

Basically, it has to run ipAccess without any problems, since the function is in the protected memory, and should enter in the interrupt (case 0x08) when I try to write 128 inside protectedVar[0]. Actually, it just write and read everything without distinctions and it doesn't enter in the interrupt at all. What am I doing wrong?

Thank you,

Marco

**Attention** This is a public forum