Hi there,
I have finished soldering my custom MSP430 board today and now would like to flash a blink program to it. (My previous MSP430 experience comes from the eZ430-F2013 and the Chronos)
I loaded the MSP430F5510 Blink sample, connected a 150Ohms Resistor between VBUS and PUR to trigger the USB BSL and connected the Board which then showed up as "Unknown Device" in the Device Manager and when looking at the device info it says that the device was stopped (Code: 43). Is that normal so far?
I then tried flashing and debugging the Blink program using CCS5, however upon starting debug, it confronted me with the error "No USB FET was found". Other threads on the topic have not been able to help me so far (e.g. changing the USB port in the general options)
I have to say that I had soldered a HTC74 chip wrong way round on to the board and upon power connect, that got really warm. After turning the chip right way round, I did some tests using a current limited power supply, everything seemed okay, so I don't think that the MSP430 was damaged by that.
Any help on this one would be great!