This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12 least significant 2 bits always 1.

Other Parts Discussed in Thread: MSP430F2618

I have an MSP430F2618 with built in 12-bit ADC, but for some reason the values it returns always end with the 2 least significant bits set to 1, except when it zeroes out. In other words, the counts are always of the form 0x##3, 0x##7, 0x##B, or 0x##F. Am I missing something in my initialization that magically turns my 12bit ADC into a 10bit? Could there be some transient voltage that just happens to always saturate the sig-delt circuit for the least significant bits? Any suggestions?

P6SEL |= 0x01; // P6.0,P6.1-ADC option select
ADC12CTL0 = SHT0_8 + ADC12ON + MSC; // Set sampling time, turn on ADC12 (256 ADC12CLK cycles, ADCON, Multiple sample and conversion)
ADC12CTL1 = SHP + CONSEQ_1; // Use sampling timer (SAMPCON signal is sourced from the sampling timer, Sequence-of-channels conversion sequence mode)
ADC12MCTL0 = SREF_6 + INCH_0 + EOS; //inch (Input channel) assigns channel to this memory location, (Reference: VR+ =VeREF+ and VR- = VREF-), end of sequence
ADC12IE = 0x01; // Enable interrupt
ADC12CTL0 |= ENC; // Conversion enabled

**Attention** This is a public forum