This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with simulation of the OPT 101 using PSPICE

Other Parts Discussed in Thread: OPT101

Hello all,

I am haveing a difficult time simulating the OPT101 with my PSPICE release 16.6.

I got a spice file with name as OPT101/BB and connected as shown

 4405.opt_spice_pic.docx

 

I want to simulate or show the output of this device when light shines on it and when it is dark, so I am using the Vsin to simulate light,

and i keep on getting error as follows


**** 08/15/13 15:09:20 ***** PSpice 16.6.0 (October 2012) ***** ID# 0 ********

 ** Profile: "SCHEMATIC1-trial5"  [ C:\Cadence\SPB_16.6\tools\capture\trial5-pspicefiles\schematic1\trial5.sim ]


 ****     CIRCUIT DESCRIPTION


******************************************************************************




** Creating circuit file "trial5.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS

*Libraries:
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\Users\billtaylor\cdssetup\OrCAD_PSpice/16.6.0/PSpice.ini file:
.lib "nom.lib"

*Analysis directives:
.TRAN  0 10m 0
.OPTIONS ADVCONV
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"



**** INCLUDING SCHEMATIC1.net ****
* source TRIAL5
V_V1         N00219 0 9Vdc
X_U1         0 N01633 N00219 0 N01090 N01090 OPT101/BB
V_V2         N01633 0  AC <AC>=7.5m
---------------------------$
ERROR(ORPSIM-16492): Missing value
+SIN <VOFF>=0 <VAMPL>=10 <FREQ>=14k 0 0 0

**** RESUMING trial5.cir ****
.END

I am not sure what I am doing wrong. please can anyone help?

**Attention** This is a public forum