This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In CCS Version: 5.4.0.00091 on Windows 7 Pro SP1 connected to an MSP-EXP430G2 LaunchPad on USB, when I attempt to rebuild and run the temperature sensor demo application (the "user experience" app) or any program, I get this error message "MSP430: Error connecting to the target: Could not find device (or device not supported)".
Prior to doing this, I had been using the MSP-EXP430FR5739 LaunchPad connected to the same machine on USB, loading and running that board's "user experience" demo app . I have two CCS workspaces, one for MSP430FR projects and one for MSP430G2 projects. CCS has no problem loading and running the MSP430FR projects on the MSP-EXP430FR5739 LaunchPad but any MSP430G2 projects that I run on theMSP-EXP430G2 LaunchPad generates the error.
Any help would be greatly appreciated.
Mark,
Have you setup Target Configuration for the MSP430G2 device? Error message sounds like CCS couldn't find the device it was looking for. If you have Target Configuration for the MSP430G2 device can you run the Connection Test successfully?
Not sure of your experience level with CCS. If you are new to CCSv5, I suggest you look at tutorial information here: http://processors.wiki.ti.com/index.php/Category:CCS_Training. The Modules Library has section on Target Configuration.
Regards.
Mark,
A couple of other things to check.
1. Check that all J3 jumpers are populated to connect onboard emulation (www.ti.com/lit/pdf/slau318, sec 4.1, pg 9).
2. Verify that the device is in the socket correctly (details in same doc as #1).
3. Can you tell if the board powers up when USB cable plugged in?
Regards.
TommyG,
Yes, the target is configured under CCS -> Project -> Properties -> General -> Family = MSP430 and Variant = MSP430G2553. The last CCS I used was 3.1 on C6x in 2008. It's Eclipsed based now I see and I've never used the MSP430. I will check the tutorial you mentioned. Thanks.
Mark
Mark,
What is the LaunchPad showing up as in Device Manager? Is the driver installing correctly? I would think it is, but have seen some issues with this on other boards lately.
John
**Attention** This is a public forum