Other Parts Discussed in Thread: ENERGIA
Hi all,
I'm working with a LaunchPad with the included G2231 and G2211 chips, and I'm experiencing the infamous "Error initializing emulator: Could not find MSP-FET430UIF on specified COM port" problem. I'm running on a Windows 8 system using CCS 5.4.0.00091, using the drivers included with the package. Here's what I've found:
- The CCS debugger sometimes will connect to the board properly and run, but this is less than half the time. Sometimes unplugging the board fixes the problem, sometimes not. When it does work, it often takes several seconds to establish the connection.
- MSP430Flasher seems to do better, but at some point will also lose connectivity with the LaunchPad, requiring the board to be unplugged and plugged back in again which usually (but not always) fixes the issue there.
- Using the GDB proxy works about as often as CCS.
- Rowley's CrossStudio for MSP-430 works *every* time, and connects almost instantly.
- Device Manager shows a properly installed and working "MSP430 Application UART" device.
- LaunchPadFirmwareUpdater2.0 seems to always find the LaunchPad, but almost always shows "No MSP430G2XXX device detected". On the rare occasion where it does work, it indicates the firmware is up to date.