This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIMBER_B PWM SINE

I read on the TI application report SLAA116 that we can use timer_b to create PWM output and then with an Analog Filter we can get a sinewave.(Figure 2. of the application report)
I am thinking  it can only generate the upper half of a sinewave as the PWM output is either zero or let's say 1 volt(IT'S AWLAYS HIGHER THAN 0).
Can we use only one I/o pin and an analog filter to create a sine wave or do we have to use two pins and combine the two halves?

Thanks in advance!

 

**Attention** This is a public forum