I got the AIR BoosterPak kit and ran them with my MSP430 launchpads, and the application GUI works good!
But now I want to look at and debug some source code, as a starting point for adapting it to custom applications. Per the instructions, I can import the ABS Air Booster Stack GUI application project from the CD, but then CCS won't let me see, for instance, the source code for main.c, displaying in the window instead'
'Error retrieving content description for resource '/CCS/Application/main.c'
and when I do a 'Build All' I get some errors... 'No rule to make target'. Of course it won't degug either. Without thinking it through, I then I loaded a simple application to blink the Launchpad LED, as a sanity check, and it loaded and ran fine. But now I am stuck, cannot load the ATC- Booster Stack GUI software back in.
I tried copying the CCS folder from the CD onto my desktop, and loading the project into Eclipse from there, but no luck.