Good day
I am building my custom PCB based on the MSP-TS430PN80USB target board. I didn't find any references for the D2 and D3 diodes. Are they mandatory?
Thank You
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good day
I am building my custom PCB based on the MSP-TS430PN80USB target board. I didn't find any references for the D2 and D3 diodes. Are they mandatory?
Thank You
Ilmars said:If they are not assembled on original board then they are not mandatory, right? After all you are building custom board - so you are in charge to define which components are needed and which are not.
In fact, they are do. That's why I am asking. I am referencing the SLAU278P document page 99.
Gaby Heifets said:I am referencing the SLAU278P document page 99.
If you (your application) need those LED's - put them on board. If you don't need them - don't put them on board. If you are not sure - put them on board with jumpers as in original circuit, later will see you use them or not. What's the problem?
I am talking about ll103A Shotky diodes. Once again D2 and D3. D2 placed after the USB VBUS entry signal. The second one placed on the JTAG power signal. Most likely they are placed to avoid back current from the MSP430, but I haven't find any reference for that.
Have you referred to the document I posted?
Thanks
The diodes are listed on page 102.
An USB-Slave should not supply power to the bus. But since this board can be external powered the diode blocks outgoing power. Normally isn’t necessary.
Pin 2 of the JTAG is the 3V supply voltage from the JTAG and for the same reason (external power) this diode. Pin 4 can be used as supply to JTAG.
**Attention** This is a public forum