Other Parts Discussed in Thread: MSP430FR5739, MSP430G2553, MSP430G2231
J6.3 (GND) – J6.3 (GND)
J2.14 (P1.6) – SV2.11 (P2.0)
J2.15 (P1.7) – SV2.8 (P2.1)
J1.6 (P1.4) – J3.7 (/RST)
J1.7 (P1.5) – J3.9 (TEST)
Theodora
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FR5739, MSP430G2553, MSP430G2231
Hi Theodora,
Thanks for providing so much information!
You are getting the Unknown command message because your script says "MASS ERASE" instead of "MASS_ERASE". Make sure there is an underscore, not a space, and then try again.
I think there is a sample script for the FR5739 included in the zip file download for the Launchpad BSL interface app note: www.ti.com/lit/zip/slaa535 that you could try.
For your question about the password, if you mass erase the part first, then the password should be all 0xff as you provided. You only need to know the password from the previous code if you are trying to be able to read back the previous code, rather than just erasing and reprogramming the device.
For your other errors, I'd try the script with the corrected MASS_ERASE command first and see if the issues persist, then post back - I'm not 100% sure what the scripter does when it encounters an unknown command and if this could throw it off.
Regards,
Katie
Hello again,
I wanted to update you on this topic.
I changed the MSP430G2553 of my launchpad to an MSP430G2231 that I borrowed earlier -which I programmed with the Firmware provided in the SLAA535a.zip-. I used the same script (after correcting the MASS_ERASE command as suggested by Katie) and the same TI-TXT file. I also used the BSL_Scripter v1.07 of slau319f.zip and it worked.
I can't tell what exactly was wrong with the MSP430G2553 firmware, but fortunately I solved my problem after changing the G2553 to a G2231 as I explained.
**Attention** This is a public forum